Everything

-MF [V3.08.00 or later]


< Compile Options / Dependency File Output Specification Options >

[Format]

-MF=file-name

 

-

[Default]

If a dependency file output specification option is specified, the dependency file is output to the current folder.

No dependency file is output unless a dependency file output specification option is specified.

[Description]

-

This option specifies the name of the dependency file to be output.

-

If the dependency file name with a path is specified, the file will be output to the specified path.

-

If a folder is specified as file-name, an error occurs.

-

If this option is specified without specifying a dependency file output specification option, an error occurs.

-

If a file with the specified name exists, the file is overwritten.