Everything

2.2 Open Realtime OS Task Analyzer Panel

Open the Realtime OS Task Analyzer panel in order to view analysis information (the state of processing program execution, the state of real-time OS resource usage, the CPU usage status, etc.).
The Realtime OS Task Analyzer panel can be opened by selecting either [View] menu >> [Realtime OS] >> [Task Analyzer 1] or [Task Analyzer 2].
Figure 2-1. Realtime OS Task Analyzer Panel
Remark Up to two Realtime OS Task Analyzer panel can be opened by selecting [View] menu >> [Realtime OS] >> [Task Analyzer 1] and then selecting [View] menu >> [Realtime OS] >> [Task Analyzer 2].