Starts CSI data transmission/reception.
Remark 1. This API function repeats the byte-level CSI transmission from the buffer specified in argument tx_buf the number of times specified in argument tx_num.
Remark 2. This API function performs byte-level CSI reception the number of times specified by the argument tx_num, and stores the data in the buffer specified by the argument rx_buf.
Remark 3. When performing a CSI reception, R_CSImn_Start must be called before this API function is called.
[Syntax]
#include “r_cg_macrodriver.h”
MD_STATUS  
R_CSImn_Send_Receive ( uint8_t * const tx_buf, uint16_t 
tx_num,
 uint8_t * const rx_buf );
Remark m is the unit number, and n is the channel number.
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       I  | 
    
       uint8_t * const tx_buf;  | 
    
       Pointer to a buffer storing the transmission data  | 
| 
       I  | 
    
       uint16_t tx_num;  | 
    
       Total amount of data to send/receive  | 
| 
       O  | 
    
       uint8_t * const rx_buf;  | 
    
       Pointer to a buffer to store the received data  | 
[Return value]
| 
       Macro  | 
    
       Description  | 
| 
       MD_OK  | 
    
       Normal completion  | 
| 
       MD_ARGERROR  | 
    
       Invalid argument specification  |