Performs processing in response to detection of overrun error.
Remark This API function is called as the callback routine of interrupt process r_uartn_interrupt_receive corresponding to the UART reception end interrupt INTSRn (process performed when the amount of data received is greater than the argument rx_num specified for R_UARTn_Receive ).
[Syntax]
#include “r_cg_macrodriver.h”
static void r_uartn_callback_softwareoverrun ( uint16_t rx_data );
Remark n is the channel number.
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       O  | 
    
       uint16_t rx_data;  | 
    
       Receive data (greater than the argument rx_num specified for R_UARTn_Receive)  | 
[Return value]
None.