Usage example
Receive 4 bytes data by UART and transmit the received data as they are. Stop UART after transmission is finished.
[GUI setting example]
| 
       Serial  | 
    
       Used  | |||
| 
       SAU0  | 
    
       Used  | |||
| 
       Channel0  | 
    ||||
| 
       Channel 0  | 
    
       UART0 (Transmission/Receive)  | |||
| 
       Data length setting (Receive)  | 
    
       8 bits  | |||
| 
       Trasfer direction setting (Receive)  | 
    
       LSB  | |||
| 
       Parity setting (Receive)  | 
    
       None  | |||
| 
       Stop bit length setting (Receive)  | 
    
       1 bit fixed  | |||
| 
       Receive data level setting  | 
    
       Normal  | |||
| 
       Transfer rate setting (Receive)  | 
    
       9600(bps) (error:+0.16% Minimum permissible value:-5.17% Maximum permissible value:+5.16%)  | |||
| 
       Reception end interrupt priority (INTSR0)  | 
    
       Low  | |||
| 
       Reception end (Callback function setting)  | 
    
       Used  | |||
| 
       Reception error (Callback function setting)  | 
    
       Used  | |||
| 
       Transfer mode setting  | 
    
       Single transfer mode  | |||
| 
       Data length setting (Transmit)  | 
    
       8 bits  | |||
| 
       Transfer direction setting (Transmit)  | 
    
       LSB  | |||
| 
       Parity setting (Transmit)  | 
    
       None  | |||
| 
       Stop bit length setting (Transmit)  | 
    
       1 bit  | |||
| 
       Transmit data level setting  | 
    
       Normal  | |||
| 
       Transfer rate setting (Transmit)  | 
    
       9600(bps) (error: +0.16%)  | |||
| 
       Transmit end interrupt priority (INTST0)  | 
    
       Low  | |||
| 
       Transmission end (Callback function setting)  | 
    
       Used  | |||
[API setting example]
r_main.c
/* Start user code for global. Do not edit comment generated here */
extern volatile uint8_t g_uart0_buf[4];
/* End user code. Do not edit comment generated here */
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Start the UART0 module operation */
R_UART0_Start();
/* Receive UART0 data */
R_UART0_Receive((uint8_t *)g_uart0_buf, 4U);
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}
r_cg_serial_user.c
/* Start user code for global. Do not edit comment generated here */
volatile uint8_t g_uart0_buf[4];
/* End user code. Do not edit comment generated here */
static void r_uart0_callback_receiveend(void)
{
/* Start user code. Do not edit comment generated here */
/* Send UART0 data */
R_UART0_Send((uint8_t *)g_uart0_buf, 4U);
/* End user code. Do not edit comment generated here */
}
static void r_uart0_callback_sendend(void)
{
/* Start user code. Do not edit comment generated here */
/* Stop the UART0 module operation */
R_UART0_Stop();
/* End user code. Do not edit comment generated here */
}