Reads the alarm conditions (weekday, hour, minute).(in the case of the binary mode setting)
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_rtc.h”
void R_RTC_Get_BinaryAlarmValue ( uint32_t * const alarm_enable,
uint32_t * const alarm_val );
[Argument(s)]
|
I/O |
Argument |
Description |
|
O |
uint32_t * const alarm_enable; |
Pointer to structure in which to store the alarm enable value being read |
|
O |
uint32_t * const alarm_val; |
Pointer to structure in which to store the conditions being read |
[Return value]
None.