Real-time clock
Below is a list of API functions output by the Code Generator for real-time clock use.
Table 3.13 API Functions: [Real-time Clock] (1)
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the real-time clock.  | |
| 
       Performs user-defined initialization relating to the real-time clock.  | |
| 
       Performs processing in response to the real-time clock interrupt INTRTC.  | |
| 
       Starts the count of the real-time clock (year, month, weekday, day, hour, minute, second).  | |
| 
       Ends the count of the real-time clock (year, month, weekday, day, hour, minute, second).  | |
| 
       Halts the clock supplied to the real-time clock.  | |
| 
       Sets the clock type (12-hour or 24-hour clock) of the real-time clock.  | |
| 
       Sets the counter value of the real-time clock.  | |
| 
       Sets the counter value of the real-time clock.(in the case of the calendar mode setting)  | |
| 
       Sets the counter value of the real-time clock.(in the case of the binary mode setting)  | |
| 
       Reads the counter value of the real-time clock.  | |
| 
       Reads the counter value of the real-time clock.(in the case of the calendar mode setting)  | |
| 
       Reads the counter value of the real-time clock.(in the case of the binary mode setting)  | |
| 
       Sets the cycle of the interrupts INTRTC, then starts the cyclic interrupt function.  | |
| 
       Ends the cyclic interrupt function.  | |
| 
       Performs processing in response to the cyclic interrupt INTRTC.  | |
| 
       Starts the alarm interrupt function.  | |
| 
       Starts the alarm interrupt function.(in the case of the calendar mode setting)  | |
| 
       Starts the alarm interrupt function.(in the case of the binary mode setting)  | |
| 
       Ends the alarm interrupt function.  | |
| 
       Sets the alarm conditions (weekday, hour, minute).  | |
| 
       Sets the alarm conditions (year, month, weekday, day, hour, minute, second).(in the case of the calendar mode setting)  | |
| 
       Sets the alarm conditions.(in the case of the binary mode setting)  | |
| 
       Reads the alarm conditions (weekday, hour, minute).  | 
Table 3.14 API Functions: [Real-time Clock] (2)
| 
       API Function Name  | 
    
       Function  | 
| 
       Reads the alarm conditions (year, month, weekday, day, hour, minute, second).(in the case of the calendar mode setting)  | |
| 
       Reads the alarm conditions.(in the case of the binary mode setting)  | |
| 
       Performs processing in response to the alarm interrupt INTRTC.  | |
| 
       Enables output of the correction clock (1 Hz) to the RTC1HZ pin.  | |
| 
       Disables output of the correction clock (1 Hz) to the RTC1HZ pin.  | |
| 
       Enables output of the RTCOUT.  | |
| 
       Disables output of the RTCOUT.  | |
| 
       Performs processing in response to the alarm interrupt INTRTCALM.  | |
| 
       Performs processing in response to the periodic interrupt INTRTCPRD.  | |
| 
       Performs processing in response to the cyclic interrupt INTRTC.  |