Sets the alarm conditions.(in the case of the binary mode setting)
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_rtc.h”
void R_RTC_Set_BinaryAlarmValue ( uint32_t alarm_enable, uint32_t alarm_val );
[Argument(s)]
|
I/O |
Argument |
Description |
|
I |
uint32_t alarm_enable; |
Alarm
enable |
|
I |
uint32_t alarm_val; |
Alarm conditions (count value) (Set the value to the Binary Counter Alarm Register) |
[Return value]
None.