Everything

R_DTCm_Stop

Prohibits starting of the data transfer controller.

Remark         In this API function, starting the data transfer controller is prohibited by operating the DTCE bit of the DTC activation enable register n (DTCERn) supporting the transfer data number m.
m is the transfer data number, n is the interrupt vector number.

 

[Syntax]

void    R_DTCm_Stop ( void );

Remark         m is the transfer data number.

 

[Argument(s)]

None.

 

[Return value]

None.