Performs processing in response to the event link interrupt.
Remark         
This API function is called to run interrupt processing for the event signal 
defined in event link setting register.
n is the source 
number.
[Syntax]
static void r_elc_elsrni_interrupt ( void );
Remark n is the source number.
[Argument(s)]
None.
[Return value]
None.