Event link controller (ELC)
Below is a list of API functions output by the Code Generator for event link controller use.
Table 3.10 API Functions: [Event Link Controller]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the event link controller.  | |
| 
       Performs user-defined initialization relating to the event link controller.  | |
| 
       Performs processing in response to the event link interrupt.  | |
| 
       Starts interlinked operation of peripheral functions.  | |
| 
       Ends interlinked operation of peripheral functions.  | |
| 
       Generates the software event.  | |
| 
       Sets the value of a port buffer.  | |
| 
       Gets the value of a port buffer.  |