This option specifies the target name.
[Specification format]
- | Interpretation when omitted |
The target name is not changed.
[Detailed description]
- | This option specifies the target name to be output to the dependency file. |
- | This option is invalid if the -MM option is not specified. |
- | If no target name is specified for the -MT option, an error occurs. |
[Example of use]
<test.asm>
$INCLUDE "inc1.inc"
$INCLUDE "inc2.inc"
|
<inc2.inc>
Note | “inc1.inc” and “inc3.inc” will be empty files. |
<Output contents>
A: test.asm
A: inc1.inc
A: inc2.inc
A: inc3.inc
|