Everything

 

-MF [V1.06.00 or later]


This option changes the name of the dependency file.

[Specification format]

-MF=file-name

 

-

Interpretation when omitted

The dependency file name is not changed. The output file name is the same as the input file name, with the extension replaced by “dep”.

[Detailed description]

-

This option changes the name of the dependency file to be output.

-

This option is invalid if the -MM option is not specified.

[Example of use]

-

To output the dependencies to “D.dep”, describe as:

asrh test.asm -MM -MF=D.dep

[Remark]

-

When multiple input files are specified, only the dependency file for the last input file is output.