This option outputs the dependency file, and then continues assembling.
[Specification format]
- | Interpretation when omitted |
No dependency file is output.
[Detailed description]
- | This option outputs the dependencies of the input file, as specified by the $INCLUDE or $BINCLUDE control instruction, to the dependency file in makefile format. It also executes assembling. |
- | The output file name is the same as the input file name, with the extension replaced by “dep”. |
[Remark]
- | When multiple input files are specified, a separate dependency file is output for each one. |