Everything

[Cyclic Handler] tab

This tab displays the cyclic handler information (e.g. Cyclic Handler Name and ID) of the RI600PX.
Figure A-25. [Cyclic Handler] Tab
The following items are explained here.
[How to open]
- From the [Debug] menu, select [Download].
- From the [View] menu, select [Realtime OS] >> [Resource Information].
[Description of each area]
(1) Information display area
This area displays the cyclic handler information (e.g. Cyclic Handler Name and ID) of the RI600PX.
This area consists of the following items.
Cyclic Handler Name
An icon indicating the current status of the cyclic handler and the name of the cyclic handler are shown in the following format.
Icon Name
Non-operational state (STP state)
Operational state (STA state)
Non-existent cyclic handler
ID
The ID of the cyclic handler is shown.
Status
The current status of the cyclic handler is shown.
TCYC_STP
Non-operational state (STP state)
TCYC_STA
Operational state (STA state)
Interval
The activation cycle of the cyclic handler is shown. A unit of the time is millisecond. But the unit is a basic clock count when a denominator of base clock interval time (tic_deno) is 1.
Phase
The initial activation phase of the cyclic handler is shown. A unit of the time is millisecond. But the unit is a basic clock count when a denominator of base clock interval time (tic_deno) is 1.
Time Left
The time left before the next activation of the cyclic handler is shown. A unit of the time is millisecond. But the unit is a basic clock count when a denominator of base clock interval time (tic_deno) is 1.
Start Address
The start address of the cyclic handler is shown.
Extended Information
The extended information of the cyclic handler is shown.
Attribute
The attributes of the cyclic handler (initial activation state and existence of saved activation phases) are shown in the following format.
Initial activation state Existence of saved activation phases
[Initial activation state of cyclic handler]
TA_STA
Operational state (STA state)
Nothing displayed
Non-operational state (STP state)
[Existence of saved activation phases]
TA_PHS
There are saved activation phases.
Nothing displayed
There are no saved activation phases.

[Context menu]
The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.
(1) Header row
Display
Displays cascade menus for selecting the header items to display.
Selected item name
The following items are displayed for selection.
Cyclic Handler Name, ID, Status, Interval, Phase, Time Left, Start Address, Extended Information, Attribute
Checked
The item in question will be displayed.
Not checked
The item in question will not be displayed.
Notation
Displays cascade menus for selecting the display notation.
Selected item name
The following items are displayed for selection.
ID, Interval, Phase, Time Left, Start Address, Extended Information
DEC
Displays value in signed decimal number.
HEX
Displays value in hexadecimal number.

(2) Footer row
Jump to Source (Start Address)
Opens the Editor panel, and displays the source code of the cyclic handler.
Jump to Disassemble (Start Address)
Opens the Disassemble panel, and displays the results of disassembling the cyclic handler.
Reset Display Item
Resets the item displayed to initial state.