Everything

[Task] tab

This tab displays the task information (e.g. Task Name and ID) of the RI600PX.
Figure A-4. [Task] Tab
The following items are explained here.
[How to open]
- From the [Debug] menu, select [Download].
- From the [View] menu, select [Realtime OS] >> [Resource Information].
[Description of each area]
(1) Information display area
(a) First layer
This layer displays the task information (e.g. Task Name and ID) of the RI600PX.
This layer consists of the following items.
Task Name
An icon indicating the current status of the task and the name of the task are shown in the following format.
Icon Name
DORMANT state
READY state
RUNNING state
WAITING state
SUSPENDED state
WAITING-SUSPENDED state
NON-EXISTENT state
ID
The ID of the task is shown.
Status
The current state of the task is shown.
Dormant
DORMANT state
Ready
READY state
Running
RUNNING state
Waiting
WAITING state
Suspended
SUSPENDED state
Waiting-Suspended
WAITING-SUSPENDED state
Non-Existent
NON-EXISTENT state
Wait Factor
The task wait factor (type of WAITING state, object ID and attribute of WAITING state) is shown in the format below.
Type of WAITING state (Object ID) Attribute of WAITING state
Note that if the current state of the task is other than WAITING state or WAITING-SUSPENDED state, "--" appears.
If the WAITING state type is sleeping state or delayed state, then "(Object ID)" is not shown.
[Type of WAITING state]
SLP
Sleeping state
DLY
Delayed state
SEM
Waiting state for a semaphore resource
FLG
Waiting state for an eventflag
SDTQ
Sending waiting state for data queue
RDTQ
Receiving waiting state for a data queue
MBX
Waiting state for a mailbox
MTX
Waiting state for a mutex
SMBF
Sending waiting state for a message buffer
RMBF
Receiving waiting state for a message
buffer
MPF
Waiting state for a fixed-sized memory pool
MPL
Waiting state for a variable-sized memory pool
[Attribute of WAITING state]
ANDW
AND waiting condition for a eventflag
ORW
OR waiting condition for a eventflag
TMO
Waiting for timeout
FIFO
Waiting for FIFO order
PRI
Waiting for task priority order
Wait Data
The request conditions triggering the task's transition to WAITING state are shown.
Note that if the task's current state is other than waiting state for an eventflag, sending waiting state for a data queue, or waiting state for a variable-sized memory block, "--" is shown.
Wait bit pattern
Waiting state for an eventflag
Data element to be sent to the data queue
Sending waiting state for a data queue
Memory block size to be acquired
Waiting state for a variable-sized memory block
Time Left
The time left until the delayed state is released is shown. A unit of the time is millisecond. But the unit is a basic clock count when a denominator of base clock interval time (tic_deno) is 1.
If the task is in the WAITING state forever, "TMO_FEVR" appears.
Note that if the current state of the task is other than WAITING state or WAITING-SUSPENDED, "--" appears.
Interrupt
"Enable" is shown.
Current Priority
The current priority of the task is shown.
Task Start Address
The start address of the task is shown.
Current PC
The current PC value of the task is shown.
Current Task SP
The current SP value of the task is shown.
Task Stack Area
The start address, end address, and size (in bytes) of the task stack are shown in the following format.
Start address - End address (Size)
Initial Priority
The initial priority of the task is shown.
Suspend Count
The suspension count of the task is shown.
Wakeup Count
The wakeup request count of the task is shown.
Activate Count
The activation request count of the task is shown.
Attribute
The attributes of the task (the task's initial activation state and initial interrupt state) are shown in the following format.
Initial activation state Initial interrupt state
[Initial activation state of task]
TA_ACT
READY state
Nothing displayed
DORMANT state
[Initial interrupt state of task]
TA_ENAINT
All interrupts are enabled at task activation.
Extended Information
The extended information of the task is shown.
Tex Start Address
The start address of the task exception handling routine is shown.
Note that if the task exception handling routine is undefined, the name will
appear as "--".
Tex Status
The current status of the task exception handling routine is shown.
Note that if the task exception handling routine is undefined, the name will
appear as "--".
TTEX_DIS
Disable task exceptions
TTEX_ENA
Enable task exceptions
Tex Request Pattern
The pending exception code of the task exception handling routine is shown.
Note that if the task exception handling routine is undefined, the name will
appear as "--".
Tex Executing Pattern
"--" is shown.
ex Attribute
"--" is shown.

(b) Second layer
See the [Mutex] tab for details about locking mutex information.
Figure A-5. [Task] Tab (Locking Mutex Information)
[Context menu]
The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.
(1) Header row
Display
Displays cascade menus for selecting the header items to display.
Selected item name
The following items are displayed for selection.
Task Name, ID, Status, Wait Factor, Wait Data, Time Left, Interrupt, Current Priority, Task Start Address, Current PC, Current Task Stack SP, Task Stack Area, Initial Priority, Suspend Count, Wakeup Count, Activate Count, Attribute, Extended Information, Tex Start Address, Tex Status, Tex Request Pattern, Tex Executing Pattern, Tex Attribute
Checked
The item in question will be displayed.
Not checked
The item in question will not be displayed.
Notation
Displays cascade menus for selecting the display notation.
Selected item name
The following items are displayed for selection.
ID, Wait Factor, Wait Data, Time Left, Current Priority, Task Start Address, Current PC, Current Task Stack SP, Task Stack Area, Initial Priority, Suspend Count, Wakeup Count, Activate Count, Extended Information, Tex Start Address, Tex Request Pattern, Tex Executing Pattern
DEC
Displays value in signed decimal number.
HEX
Displays value in hexadecimal number.

(2) Footer row
Jump to Source (Task Start Address)
Opens the Editor panel, and displays the source code of the task.
Jump to Disassemble (Task Start Address)
Opens the Disassemble panel, and displays the results of disassembling the task.
Jump to Source (Current PC)
Opens the Editor panel, and displays the contents of the Current PC.
Jump to Disassemble (Current PC)
Opens the Disassemble panel, and displays the contents of the Current PC.
Jump to Memory (Current Task SP)
Opens the Memory panel, and displays the contents of the Current Task SP.
Jump to Source (Tex Start Address)
Opens the Editor panel, and displays the source code of the task exception handling routine.
Jump to Disassemble (Tex Start Address)
Opens the Disassemble panel, and displays the results of disassembling the task exception handling routine.
Reset Display Item
Resets the item displayed to initial state.