Everything

[Message Buffer] tab

This tab displays the message buffer information (e.g. Message Buffer Name and ID) of the RI600PX.
Figure A-19. [Message Buffer] Tab
The following items are explained here.
[How to open]
- From the [Debug] menu, select [Download].
- From the [View] menu, select [Realtime OS] >> [Resource Information].
[Description of each area]
(1) Information display area
(a) First layer
This layer displays the message buffer information (e.g. Message Buffer Name and ID) of the RI600PX.
This layer consists of the following items.
Message Buffer Name
An icon indicating the current status of the message buffer and the name of the message buffer are shown in the following format.
Icon Name
There are sending waiting tasks.
There are receiving waiting tasks.
There are receiving waiting messages.
There are no waiting tasks/receiving waiting messages.
Non-existent message buffer
ID
The ID of the message buffer is shown.
Queue Status
The current status of the message buffer is shown.
Waiting Tasks (Send)
There are sending waiting tasks.
Waiting Tasks (Receive)
There are receiving waiting tasks.
Waiting Messages
There are receiving waiting messages.
Empty
There are no waiting tasks/receiving waiting messages.
Top Address
The start address of the message buffer is shown.
Total Buffer Size
The total buffer size (in bytes) of the message buffer is shown.
Free Buffer Size
The free buffer size (in bytes) of the message buffer is shown.
Maximum Message Size
The maximum message size (in bytes) of the message buffer is shown.
Number of Message
The number of message stored in the message buffer.
Attribute
Displays the queuing method of the sending waiting tasks.
TA_TFIFO
FIFO order

(b) Second layer
<1> Waiting task information
The waiting task information (e.g. Task Name and ID) only appears if there are tasks queued in the message buffer's wait queue.
See the [Task] tab for details about waiting task information.
Figure A-20. [Message Buffer] Tab (Waiting Task Information)
[Context menu]
The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.
(1) Header row
Display
Displays cascade menus for selecting the header items to display.
Selected item name
The following items are displayed for selection.
Message Buffer Name, ID, Queue Status, Top Address, Total Buffer Size, Free Buffer Size, Maximum Message Size, Number of Message, Attribute
Checked
The item in question will be displayed.
Not checked
The item in question will not be displayed.
Notation
Displays cascade menus for selecting the display notation.
Selected item name
The following items are displayed for selection.
ID, Top Address, Total Buffer Size, Free Buffer Size, Maximum Message Size, Number of Message
DEC
Displays value in signed decimal number.
HEX
Displays value in hexadecimal number.

(2) Footer row
Jump to Memory (Top Address)
Opens the Memory panel, and displays the contents of the message buffer.
Reset Display Item
Resets the item displayed to initial state.