|
debugger.ActionEvent.Enable
|
This function enables an action event setting.
[Specification format]
debugger.ActionEvent.Enable(actionEventNumber = "")
|
[Argument(s)]
|
|
|
|
actionEventNumber
|
Specify the action event number to enable.
|
[Return value]
If an action event setting was enabled successfully: True
If there was an error when enabling an action event setting: False
[Detailed description]
- | This function enables the action event specified by actionEventNumber. |
- | If actionEventNumber is not specified, then events of all action event numbers will be enabled. |
[Example of use]
>>>debugger.ActionEvent.Enable(1)
True
>>>debugger.ActionEvent.Enable()
True
>>>
|