Everything

debugger.Performance.Disable


This function disables performance measurement. [RH850][E1/E2/E2 Lite/E20/Full-spec emulator/IE850A]

[Specification format]

debugger.Performance.Disable(performanceNumber = "")

[Argument(s)]

Argument

Description

performanceNumber

Specify the performance measurement event number to disable.

[Return value]

If performance measurement was disabled successfully: True

If there was an error when disabling performance measurement: False

[Detailed description]

-

This function disables performance measurement of a performance measurement event number specified by performanceNumber.

-

If performanceNumber is not specified, then performance measurement of all performance measurement event numbers will be disabled.

[Example of use]

>>>debugger.Performance.Disable(1)
True
>>>