|
|
|
|
build.Assemble.AssembleListFileOutputFolder
|
This property is for setting or referring to the folder for the output of assembly listing files. It is an assembly option for the active project.
|
|
build.Assemble.OutputAssembleListFile
|
This property is for setting or referring to whether to output assembly listing files. It is an assembly option for the active project.
|
|
build.Common.DataEndian
|
This property is for setting or referring to the endian of data. It is a common option for the build tool for the active project.
|
|
build.Common.IntermediateFileOutputFolder
|
This property is for setting or referring to the folder for the output of intermediate files. It is a common option for the build tool for the active project.
|
|
build.Common.MergedErrorMessageFileOutputFolder
|
This property is for setting or referring to the folder for the output of error message merge files. It is a common option for the build tool for the active project.
|
|
build.Common.MergeErrorMessageFile
|
This property is for setting or referring to whether to merge error message files. It is a common option for the build tool for the active project.
|
|
build.Common.PrecisionOfDoubleType
|
This property is for setting or referring to the precision used with double and long double types. It is a common option for the build tool for the active project.
|
|
build.Common.UseDPFPU
|
This property is for setting or referring to whether to use double-precision floating-point operation instructions. It is an assembly option for the active project.
|
|
build.Compile.AdditionalOptions
|
This property sets or refers to the compile options for the active project regarding other additional options.
|
|
build.Compile.AssemblySourceFileOutputFolder
|
This property is for setting or referring to the folder for the output of assembly source files. It is a compile option for the active project.
|
|
build.Compile.FloatType
|
This property is for setting or referring to the method of floating-point calculation. It is a compile option for the active project.
|
|
build.Compile.IncludePath
|
This property sets or refers to the compile options for the active project regarding additional include paths.
|
|
build.Compile.ListFileOutputFolder
|
This property is for setting or referring to the folder for the output of assembly listing files. It is a compile option for the active project.
|
|
build.Compile.Macro
|
This property sets or refers to the compile options for the active project regarding defined macros.
|
|
build.Compile.OutputAssemblySourceFile
|
This property is for setting or referring to whether to output assembly source files. It is a compile option for the active project.
|
|
build.Compile.OutputListFile
|
This property is for setting or referring to whether to output assembly listing files or source listing files. It is a compile option for the active project.
|
|
build.Compile.PrecisionOfDoubleType
|
This property is for setting or referring to the precision of double type and long double type. It is a compile option for the active project.
|
|
build.Compile.PreprocessedSourceFileOutputFolder
|
This property is for setting or referring to the folder for the output of preprocessed source files. It is a compile option for the active project.
|
|
build.HexOutput.OutputFolder
|
This property is for setting or referring to the folder for hexadecimal output. It is a hexadecimal output option for the active project.
|
|
build.IsBuilding
|
This property confirms whether a build is running.
|
|
build.Library.EnableMathfH
|
This property is for setting or referring to whether or not mathf.h (C89/C99) is enabled. It is a library generate option for the active project.
|
|
build.Library.EnableMathH
|
This property is for setting or referring to whether or not math.h (C89/C99) is enabled. It is a library generate option for the active project.
|
|
build.Link.AdditionalOptions
|
This property sets or refers to the link options for the active project regarding other additional options.
|
|
build.Link.LibraryFile
|
This property sets or refers to library files of the active project.
|
|
build.Link.OutputFolder
|
This property is for setting or referring to the folder for the output of the results of linkage of the object files from the active project. It is a linker option for the active project.
|
|
build.Link.RangeOfDebugMonitorArea
|
This property is for setting or referring to the range of a debug monitoring area. It is a link option for the active project.
|
|
build.Link.SectionAlignment
|
This property sets or refers to the link options for the active project regarding section alignment.
|
|
build.Link.SectionROMtoRAM
|
This property sets or refers to the link options for the active project regarding sections where symbols are mapped from ROM to RAM.
|
|
build.Link.SectionStartAddress
|
This property sets or refers to the link options for the active project regarding the addresses where sections start.
|
|
build.Link.SectionSymbolFile
|
This property sets or refers to the link options for the active project regarding sections whose external defined symbols are to be output to a file.
|
|
build.Link.SetDebugMonitorArea
|
This property is for setting or referring to whether or not a debug monitoring area is set. It is a link option for the active project.
|
|
build.ROMization.OutputObjectFile
|
This property sets or refers to the setting for output of a ROMized object file, that is, the value of the ROMization process option for the active project.
|
|
build.Version
|
This property is for setting or referring to the version of the compiler package that is in use for the active project.
|