This property is for setting or referring to the method of floating-point calculation. It is a compile option for the active project. [CC-RH]
|
Generates floating-point calculation instructions of FPU for floating-point calculations. |
||
|
Generates runtime library call instructions for floating-point calculations. |
||
This property is for setting or referring to the method of floating-point calculation. It is a compile option for the active project. |