This property is for setting or referring to whether to merge error message files. It is a common option for the build tool for the active project. [CC-RH] [CC-RL]
If error message files are to be merged: True
If error message files are not to be merged: False
If the compiler is not supported: None
This property is for setting or referring to whether to merge error message files. It is a common option for the build tool for the active project. |