CcnvCA78K0は,78K0マイクロコントローラ用CコンパイラであるCA78K0,CC78K0(以降は,CA78K0とCC78K0をまとめてCA78K0と記述します)の開発環境で作成したCソース・プログラムを,RL78ファミリ用CコンパイラであるCC-RLで動作するCソース・プログラムに変換する,Cソースコンバータです。Cソース中に記述したCA78K0用拡張機能を,CC-RL用拡張機能に変換します。
CcnvCA78K0は,CA78K0用プログラムからCC-RL用プログラムへの移行を支援するためのソフトウェアです。変換後のプログラムが完全に動作することは保証しません。必ず変換後のCソースを用いてプログラムの動作確認をしてください。