文字列を整数(unsigned long int型)へ変換し,最終文字列へのポインタを格納します。
unsigned long int __far strtoul(const char __near *nptr, char __near * __near *endptr, int base);(C90)
unsigned long int __far strtoul(const char __near * restrict nptr, char __near * __near * restrict endptr, int base);(C99) 【V1.07以降】
unsigned long int __far _COM_strtoul_ff(const char __far *nptr, char __far * __far *endptr, int base);(C90)
unsigned long int __far _COM_strtoul_ff(const char __far * restrict nptr, char __far * __far * restrict endptr, int base);(C99) 【V1.07以降】
部分文字列が変換できた場合,変換された値を返します。変換できなかった場合,0を返します。
オーバフローが生じる場合,ULONG_MAXを返し,マクロERANGEをグローバル変数errnoに設定します。
nptrの指す文字列の先頭から0個以上の空白類文字(isspace関数が真となる文字)の列を読み飛ばし,次の文字からの文字列をunsigned long int型の表現に変換します。baseが0である場合はCの基数表現と解釈し,baseが2以上36以下である場合はその値を基数とします。endptrがnullポインタでない場合は変換されなかった残りの文字列へのポインタをendptrに設定します。