New Toolbar dialog box


This dialog box is used to create a new toolbar to appear in the Main window.

Figure A.64

New Toolbar Dialog Box

 

The following items are explained here.

[How to open]

-

In the [Toolbars] tab of the User Setting dialog box, click the [New...] button.

[Description of each area]

(1)

[Toolbar name]

Type in the name of the new toolbar directly via the keyboard.

"UltraToolbar1" is specified by default.

(2)

[Location]

Select the location for the new toolbar from the following drop-down list.

The location specified here is the location where the new toolbar will appear immediately after it is created (toolbars can be moved freely by dragging and dropping).

Docked Top

Displays the toolbar at the top of the Main window (default).

Docked Bottom

Displays the toolbar at the bottom of the Main window.

Docked Left

Displays the toolbar on the leftedge of the Main window.

Docked Right

Displays the toolbar on the rightedge of the Main window.

Floating

Displays the toolbar above the Main window, without docking it.

[Function buttons]

Button

Function

OK

Creates a new toolbar with the specified information, and closes this dialog box.

The new toolbar appears in the list on the User Setting dialog box’s [Toolbars] tab, with its check box selected.

Cancel

Ignores the setting and closes this dialog box.