Below is a list of the windows, panels, and dialog boxes related to the basic operations of CS+ and the procedure of build using CS+.
This is the start-up window that opens when CS+ is launched. |
|
This panel allows you to easily open a tutorial, access (create/open) a project, or load a sample project. |
|
This dialog box is used to create new projects or subprojects. |
|
This dialog box configures the composition files of the source project (the source files and the like) to convert them for the build tool of the project to be created. |
|
This dialog box includes the settings for conversion from e2 studio and the old development environment (CubeSuite, HEW, PM+) project (or workspace) to a CS+ project. |
|
This panel is used to display components of the microcontroller, build tool, and source file of the project in tree view. |
|
This dialog box is used to change the microcontroller to be used in the project. |
|
This dialog box is used to create a new file and add it to the project. |
|
This dialog box is used to add existing files and folder hierarchies to the project. |
|
In this panel, the detailed information on the node that is selected in the Project Tree panel is displayed categorized. Also, the settings of the selected node can be changed. |
|
This dialog box is used to input and edit characters in one line. |
|
This dialog box is used to input and edit texts in multiple lines. |
|
This dialog box is used to edit or add the path or file name including the path. |
|
This panel is used to list various documents (user's manuals, technical updates, application notes, and tool news) related to the device selected for the active project and allow downloading of sample code, if any, that comes with the applicable application notes. |
|
This panel allows you to search through information on registers given in hardware manuals. |
|
This panel is used to display the message that is output from the build tool/debug tool/each plug-in or the result of the Find In Files with the Find and Replace dialog box. |
|
This panel is used to list the information of messages output from the build tool (error information). |
|
This panel is used to display the memory mapping information of load modules collected by the build tool. The amount of used memory can be reduced by analyzing the information. |
|
This dialog box is used to sort, show/hide the columns displayed on the Memory Mapping Profiler panel. If the display in the panel has been customized, all of those customizations can be returned to the default state in this dialog box. |
|
This dialog box is used to set filtering conditions for display of memory mapping information on the Memory Mapping Profiler panel or variable access information on the Functions and Variables Access Table panel. |
|
This dialog box is used to reference/set the dependent projects. |
|
This dialog box is used to collectively output quality-related information such as a list of source files, build option settings, information on functions and variables, and coverage rates. |
|
This dialog box is used to refer object module files and library files to be input to the linker and configure these link orders. |
|
This dialog box is used to measure and compare the ROM size or execution speed for the case in which the build options recommended by the build tool are applied. |
|
This dialog box is used to add and delete build modes and configure the current build mode in batch. |
|
This dialog box is used to do build, rebuild and clean process in batch with the build mode that the project has. |
|
This dialog box is used to display how the process has been progressed when the time consuming process is taken place. |
|
This dialog box is used to display messages output by the various tools. |
|
This dialog box is used to pack and save the project and this product. |
|
This dialog box is used to set the plug-ins to be read in when this product is started. |
|
This dialog box allows you to customize toolbars and menus displayed in the Main window. |
|
This dialog box is used to create a new toolbar to appear in the Main window. |
|
This dialog box is used to edit the name of a toolbar created by the user. |
|
This dialog box is used to assign shortcut keys to the various commands. |
|
This dialog box allows you to change the arrangement (including addition and deletion) of menu items and buttons in the Main window. |
|
This dialog box is used to select one of the divide panels shown in the Main window to activate or close. |
|
This dialog box is used to display versions of CS+ and each plug-in product. |
|
This dialog box is used to display detail version information of this product and the present project information. |
|