This panel allows you to search through information on registers given in hardware manuals. You can also automatically acquire information on a desired register by placing the cursor over the register name in the Editor, Disassemble, SFR (for RL78), IOR (for RX), or Watch panel.
The hardware manual (RL78) or register information file (RX) for the target device is automatically downloaded from the Renesas Web site and stored in the [SmartManual Docs] folder within the project folder. |
Check the Smart Browser panel to see whether you have the latest versions of hardware manuals and technical updates. The hardware manuals that have been downloaded to the [SmartManual Docs] folder may be older than the latest versions available in the Smart Browser panel. |
The following items are explained here.
With ON, place the mouse cursor over the name of an I/O register listed in the Editor, Disassemble, SFR (for RL78), IOR (for RX), or Watch panel while the Smart Manual panel is being hidden by the auto-hide feature as described in "2.10.1 Automatically hide panels" |
This panel will be hidden again if you press the [ESC] key or move the caret or focus from the panel. |
This area shows the target device that includes the register displayed in the manual area.
This area shows the information that CS+ has found regarding the register.
Be sure to read the disclaimer in relation to the information being displayed.
You can open the disclaimer by clicking on the corresponding toolbar button (see the table below). |
Copyright Pieter van Ginkel (C) 2012-2015
https://github.com/pvginkel/PdfiumViewer
This software includes the work that is distributed in the Apache License 2.0.