Everything

TraceInfo.CreateOtherDict


This function converts the value of TraceInfo.Other into the dict type. [IECUBE] [IECUBE2] [Simulator]

[Specification format]

traceInfo.CreateOtherDict()

[Argument(s)]

None

[Return value]

Object produced by converting the value of TraceInfo.Other into the dict type (for details of TraceInfo.Other, see the description of the TraceInfoTraceInfo class.)

[Detailed description]

This function converts the value of TraceInfo.Other into the dict type.

[Example of use]

>>>info = debugger.Trace.Get(1)
     1853 00h00min00s003ms702µs000ns 0x000003c2 jarl _errfunc, lp
>>>print info[0].Other
Guest,GPID=0,SPID=2
>>>print info[0].CreateOtherDict()
{'SPID': '2', 'GPID': '0', 'Guest': ''}