Everything

debugger.Map.Information


This function displays map information.

[Specification format]

debugger.Map.Information()

[Argument(s)]

None

[Return value]

List of map information (see the MapInfo class for detail)

[Detailed description]

-

This function displays map information.

number: start-address end-address access-size memory-type

[Example of use]

>>>debugger.Map.Information()
1: 0x00000000 0x0005FFFF 32 (Internal ROM area)
2: 0x00060000 0x03FF6FFF 8 (Non map area)
3: 0x03FF7000 0x03FFEFFF 32 (Internal RAM area)
4: 0x03FFF000 0x03FFFFFF 8 (SFR)
>>>