This property is for setting or referring to the endian of data. It is a common option for the build tool for the active project.[CC-RX]
[Specification format]
build.Common.DataEndian = endianType
|
[Setting(s)]
|
|
endianType
|
Specify the endian of data.
The specifiable types are listed below.
|
|
|
EndianType.Big
|
The byte order of data is big endian.
|
EndianType.Little
|
The byte order of data is little endian.
|
[Reference]
Set value
[Detailed description]
- | This property is for setting or referring to the endian of data. It is a common option for the build tool for the active project. |
[Example of use]
>>>build.Common.DataEndian = EndianType.Little
>>>print build.Common.DataEndian
Little
>>>
|