Everything

build.Compile.PreprocessedSourceFileOutputFolder


This property is for setting or referring to the folder for the output of preprocessed source files. It is a compile option for the active project. [CC-RH] [CC-RL]

[Specification format]

build.Compile.PreprocessedSourceFileOutputFolder = folder

[Setting(s)]

Setting

Description

folder

Set the path to the folder for the output of preprocessed source files as strings.

[Reference]

Path to the folder for the output of preprocessed source files

[Detailed description]

-

This property is for setting or referring to the folder for the output of preprocessed source files. It is a compile option for the active project.

[Example of use]

>>>build.Compile.PreprocessedSourceFileOutputFolder = "/ProjectDir/Output_Vx.xx.xx"
>>>print build.Compile.PreprocessedSourceFileOutputFolder
%ProjectDir%\Output_Vx.xx.xx
>>>