Everything

build.Link.SectionROMtoRAM


This property sets or refers to the link options for the active project regarding sections where symbols are mapped from ROM to RAM. [CC-RH][CC-RX][CC-RL]

[Specification format]

build.Link.SectionROMtoRAM = sectionlist

[Setting(s)]

Setting

Description

sectionlist

Set the section that maps symbols from ROM to RAM as a list of strings.

[Reference]

List of the section that maps symbols from ROM to RAM

[Detailed description]

-

This property sets or refers to the link options for the active project regarding sections where symbols are mapped from ROM to RAM.

-

Add or change for the referred list to change the setting.

[Example of use]

>>>sec = build.Link.SectionROMtoRAM     ... Refer the current setting and add the section that maps symbols from ROM to RAM
>>>print sec
['D=R', 'D_1=R_1', 'D_2=R_2']
>>>sec.append('D_3=R_3')
>>>build.Link.SectionROMtoRAM = sec
>>>print build.Link.SectionROMtoRAM
['D=R', 'D_1=R_1', 'D_2=R_2', 'D_3=R_3']