Everything
2.19.4.1 Edit execution-related events

The address condition and pass count condition [Simulator] for execution-related events you have set can be edited.

Perform this operation in the Detail dialog box (for execution events) that is opened by selecting [Edit Condition...] from the context menu after moving the caret to an execution-related eventNote you want to edit on the Events panel.

Note

An execution-related event refers to any one of the following events in the Events panel.

-

Hardware Break event (execution type)

-

Execution-related event as start and end condition in detailed information on Trace event

-

Execution-related event as start and end condition in detailed information on Timer Result event

-

Execution-related event as start and end condition in detailed information on Performance Measurement event

For the execution-related events that were set according to the descriptions in 2.11.3.1 Set a breakpoint, 2.11.4.1 Set a break event (execution type), 2.14.3.1 Set a Trace event, 2.15.2.1 Set a Timer Result event, and 2.16.1.1 Set a Performance Measurement event the initial values of the address and pass count conditions are listed below.

Table 2.23

Initial Values of Address Conditions

Item

Initial Value

Hardware Break

Trace,

Timer Result,

Performance Measurement

Compare condition

Before execution:

Specified address (==)

After execution:

Inside the range (<=Addresses<=)

Inside the range (<=Addresses<=)

Address

Address at the time of setting the event

Start address

Address at the time of setting the event

End address

Address at the time of setting the event

Use the address mask

No

Mask value

0xFFFFFFFF

Table 2.24

Initial Values of Pass count conditions

Item

Initial Value

Pass count [Simulator]

1