Everything
 

Detail dialog box (for execution events)


This dialog box is used to display and modify detailed information on an execution-related event selected in the Events panel.

Figure A.42

Detail Dialog Box (for Execution Events) [Full-spec emulator][E1][E20]

Figure A.43

Detail Dialog Box (for Execution Events) [Simulator]

 

This section describes the following.

[How to open]

-

On the Events panel, move the caret to any one of the following events, and then select [Edit Condition...] from the context menu.

-

Hardware Break event (execution type)

-

Execution-related event as start and end condition in detailed information on Trace event

-

Execution-related event as start and end condition in detailed information on Timer Result event

-

Execution-related event as start and end condition in detailed information on Performance Measurement event

[Description of each area]

(1)

Event conditions setting area

(a)

[Address Condition]

Specify the address condition.

Compare condition

Specify the condition to compare address.

[Full-spec emulator][E1][E20]

The condition for an access event being generated varies with the value of this setting.

[Specified address (==)]

: Before Execution

[Inside the range (<=Addresses<=)] / [Outside the range !(<=Addresses<=)]

: After Execution

Default

The current set value

Modifying

Select from the drop-down list

Available values

Specified address (==)

Specifies the address with [Address].

Greater than or equal to (>=)

[Simulator]

Less than or equal to (<=)

[Simulator]

Inside the range (<=Addresses<=)

Specifies the range with [Start address] and [End address].

Outside the range !(<=Addresses<=)

Address

Specify the address.

This item appears only when [Specified address (==)], [Greater than or equal to (>=)] or [Less than or equal to (<=)] is selected in [Compare condition].

Default

The current set value

Modifying

Directly enter from the keyboard.

Available values

Address expression within the valid range

Start address

Specify the start address.

This item appears only when [Inside the range (<=Addresses<=)] or [Outside the range !(<=Addresses<=)] is selected in [Compare condition].

Default

The current set value

Modifying

Directly enter from the keyboard.

Available values

Address expression within the valid range

End address

Specify the end address.

This item appears only when [Inside the range (<=Addresses<=)] or [Outside the range !(<=Addresses<=)] is selected in [Compare condition].

Default

The current set value

Modifying

Directly enter from the keyboard.

Available values

Address expression within the valid range

Use the address mask

Specify whether to specify an address mask.

This item appears only when [Specified address (==)] is selected in [Compare condition].

Default

The current set value

Modifying

Select from the drop-down list

Available values

Yes

Specifies an address mask.

No

Does not specify an address mask.

Mask value

Specify the value of address mask.

This item appears only when [Use the address mask] is set to [Yes].

Default

The current set value

Modifying

Directly enter from the keyboard.

Available values

Hexadecimal number up to five digits

(b)

[Pass Count] [Simulator]

Specify the pass count condition.

Pass count

Specify a pass count.

The relevant event occurs when the event condition is met as many times as the specified pass count.

Default

The current set value

Modifying

Directly enter from the keyboard.

Available values

1 to 32768 in decimal number

(2)

Description area

This area displays a simple description of the item selected in the Event conditions setting area.

[Toolbar]

 

Displays all categories in the Event conditions setting area.

 

Hides categories in the Event conditions setting area and rearranges only setting items in the ascending order

 

This button is always invalid.

[Function buttons]

Button

Function

OK

Applies detailed settings made in this dialog box to execution-related events and closes this dialog box.

Cancel

Cancels the save and closes this dialog box.

Help

Displays the help for this dialog box.