Performs processing in response to the DALI transmission end interrupt INTSTDLn.
This API function is called as the callback routine of interrupt process r_dalin_interrupt_send corresponding to the DALI transmission end interrupt INTSTDLn (performed when number of transmission data specified by R_DALIn_Send argument tx_num has been completed).  |