Renesas Electronics
Below is a list of API functions output by the Code Generator for serial array unit 4 (DALI/UART4) use.
Table 3.30
API Functions: [Serial Array Unit 4]
API Function Name
Function
R_DALIn_Create
Performs initialization necessary to control the serial array unit 4 (DALI/UART4).
r_dalin_interrupt_send
Performs processing in response to the DALI transmission end interrupt INTSTDLn.
r_dalin_interrupt_receive
Performs processing in response to the DALI reception end interrupt INTSRDLn.
r_dalin_interrupt_error
Performs processing in response to the DALI reception error interrupt INTSREDLn.
R_DALIn_Start
Sets DALI communication to standby mode.
R_DALIn_Stop
Ends DALI communication.
R_DALIn_Send
Starts DALI data transmission.
R_DALIn_Receive
Starts DALI data reception.
r_dalin_callback_sendend
r_dalin_callback_receiveend
r_dalin_callback_error
r_dalin_callback_softwareoverrun
Performs processing in response to detection of overrun error.