Performs processing in response to the DALI reception error interrupt INTSREDLn.
Remark  | This API function is called as the interrupt process corresponding to the DALI reception error interrupt INTSREDLn.  | 
 
[Syntax]
CA78K0R Compiler
__interrupt static  void    r_dalin_interrupt_error ( void ); 
 | 
 
 
CC-RL Compiler
static  void  __near r_dalin_interrupt_error ( void ); 
 | 
 
Remark  | n is the channel number.  | 
 
[Argument(s)]
None.
[Return value]
None.