r_dalin_callback_softwareoverrun


Performs processing in response to detection of overrun error.

Remark

This API function is called as the callback routine of interrupt process r_dalin_interrupt_receive corresponding to the DALI reception end interrupt INTSRDLn (process performed when the amount of data received is greater than the argument rx_num specified for R_DALIn_Receive).

[Syntax]

#include    "r_cg_macrodriver.h"
static  void    r_dalin_callback_softwareoverrun ( uint16_t rx_data );

Remark

n is the channel number.

[Argument(s)]

I/O

Argument

Description

O

uint16_t  rx_data;

Receive data (greater than the argument rx_num specified for R_DALIn_Receive)

[Return value]

None.