R_TAUm_Channeln_Lower8bits_Stop


Ends the count (lower 8-bit) for channel n.

Remark

This API function can only be called when the timer array unit is used as a 8-bit timer.

[Syntax]

void    R_TAUm_Channeln_Lower8bits_Stop ( void );

Remark

m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.