|
R_TAUm_Channeln_Higher8bits_Start
|
Starts the count (higher 8-bit) for channel n.
Remark | This API function can only be called when the timer array unit is used as a 8-bit timer. |
[Syntax]
void R_TAUm_Channeln_Higher8bits_Start ( void );
|
Remark | m is the unit number, and n is the channel number. |
[Argument(s)]
None.
[Return value]
None.