|
r_taum_channeln_interrupt
|
Performs processing in response to the timer interrupt INTTMmn.
Remark | This API function is called as the interrupt process corresponding to the timer interrupt INTTMmn. |
[Syntax]
CA78K0R Compiler
__interrupt static void r_taum_channeln_interrupt ( void );
|
CC-RL Compiler
static void __near r_taum_channeln_interrupt ( void );
|
Remark | m is the unit number, and n is the channel number. |
[Argument(s)]
None.
[Return value]
None.