Starts the count for channel n.
Remark | The time from the call to this API function to the start of counting depends on the type of the function in question (e.g. interval timer, square-wave output, or external event counter). |
[Syntax]
void R_TAUm_Channeln_Start ( void );
|
Remark | m is the unit number, and n is the channel number. |
[Argument(s)]
None.
[Return value]
None.