Renesas Electronics
R_S12ADn_Create_UserInit
Performs user-defined initialization relating to the 12-bit A/D converter.
Remark
This API function is called as the R_S12ADn_Create callback routine.
[Syntax]
void R_S12ADn_Create_UserInit ( void );
n is the unit number.
[Argument(s)]
None.
[Return value]