Renesas Electronics
R_S12ADn_Set_CompareValue
Sets compare level.
[Syntax]
void R_S12ADn_Set_CompareValue ( ad_channel_t reg_value0, rad_channel_t reg_value1 );
Remark
n is the unit number.
[Argument(s)]
I/O
Argument
Description
I
ad_chanel_t reg_value0
Register value set to the compare revel register 0
ad_chanel_t reg_value1
Register value set to the compare revel register 1
[Return value]
None.