Performs processing in response to the A/D scan end interrupt.
Remark | This API function is called to run interrupt processing for the A/D scan end interrupt, which is generated on completion of scanning of the analog inputs. |
[Syntax]
static void r_s12adn_interrupt ( void );
|
Remark | n is the unit number. |
[Argument(s)]
None.
[Return value]
None.