Renesas Electronics
Below is a list of API functions output by the Code Generator for 12-bit A/D converter use.
Table 3.30
API Functions: [12-Bit A/D Converter]
API Function Name
Function
R_S12ADn_Create
Performs initialization necessary to control the 12-bit A/D converter.
R_S12ADn_Create_UserInit
Performs user-defined initialization relating to the 12-bit A/D converter.
r_s12adn_interrupt
Performs processing in response to the A/D scan end interrupt.
r_s12adn_groupb_interrupt
Performs processing in response to the group B scan end interrupt.
R_S12ADn_Start
Starts A/D conversion.
R_S12ADn_Stop
Ends A/D conversion.
R_S12ADn_Get_ValueResult
Gets the result of conversion.
R_S12ADn_Set_CompareValue
Sets compare level.
r_s12adn_compare_interrupt
Performs processing in response to the compare interrupt.