-DEBug


This option outputs debug information to the output file.

[Specification format]

-DEBug

 

-

Interpretation when omitted

The debug information is output to the output file (It is the same result as when the -debug option is specified).

[Detailed description]

-

This option outputs debug information to the output file.

[Example of use]

-

To output debug information to the output file, describe as:

>rlink a.obj b.obj -debug -output=c.abs

[Remark]

-

If the -form={object|library|hexadecimal|stype|binary}, -strip option or -extract option is specified, this option will be invalid.

-

If two or more output file names are specified using the -form=absolute option and -output option, the debug information will not be output.