This option notifies the user of the external defined symbol that is not referenced.
This option notifies the user of the external defined symbol that is not referenced during link processing through an output message. |
The a message may be output for the function that inline expansion was performed during compilation. |
If there are references to constant symbols within the same file, references are not correctly analyzed so that information notified by the output messages will be incorrect. |