-RECord


This option specifies the size of the data record to be output.

[Specification format]

-RECord={record}

 

-

Interpretation when omitted

Various data records are output according to each address.

[Detailed description]

-

This option outputs data with data record record regardless of the address range.

-

The items that can be specified as record are shown below.

H16

HEX record

H20

Expanded HEX record

H32

32-bit HEX record

S1

S1 record

S2

S2 record

S3

S3 record

 

-

If there is an address that is larger than the specified data record, the appropriate data record is selected for the address.

[Example of use]

-

To output 32-bit HEX record regardless of the address range:

>rlink a.obj b.obj -record=H32 -form=hexadecimal -output=c.hex

[Remark]

-

If the -form={hexadecimal|stype} option is not specified, this option will be invalid.

-

An error will occur if the -record={S1|S2|S3} option is specified when the -form=hexadecimal option is specified, or if the -record={H16|H20|H32} option is specified when the -form=stype option is specified.