-NODEBug


This option does not output the debug information.

[Specification format]

-NODEBug

 

-

Interpretation when omitted

The debug information is output to the output file (It is the same result as when the -debug option is specified).

[Detailed description]

-

This option does not output the debug information.

[Example of use]

-

Not to output the debug information, describe as:

>rlink a.obj b.obj -nodebug -output=c.abs

[Remark]

-

If the -form={object|library|hexadecimal|stype|binary}, -strip option or -extract option is specified, this option will be invalid.